Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
There are two opportunities to make preview images available which are both controlled via the GENERATEMISSING key:
Generate missing preview images automatically (default)
[PREVIEWIMPORT] GENERATEMISSING=1
The following settings options are available:
Color scheme for preview images
[PREVIEWIMPORT] COLORSCHEME=blank
Possible values: All block names in $CADENAS_USER/colorschemes.cfg (8.1, 9.0, Purist, Metal, Wood, CAD: Catia V5, CAD: SolidEdge, CAD: SolidWorks, CAD: Unigraphics, CAD: OneSpace Designer, CAD: Pro/ENGINEER, CAD: Inventor, blank, 2D)
[PREVIEWIMPORT] SCENEVIEW=ISOMETRIC
Values: FRONT, BACK, LEFT, RIGHT, TOP, BOTTOM, ISOMETRIC, DIMETRIC, TRIMETRIC
Width of image to be created (only used if "convert" or "generateMissing" are equal to '1')
If "convert" equals '0', then the available preview images are used in the original size (independent of the set value).
Height of image to be created. This specification only works if "convert" or "generateMissing" are equal to '1'.
If "convert" equals '0', the available preview images are used in the original size (independent of the set value).
Caution | |
---|---|
For the generation, OpenGL must be available, which is usually the case! If the Classimporter is carried out as "planned task", this may not be the case. |
Import existing preview images
[PREVIEWIMPORT] GENERATEMISSING=0
Note | |
---|---|
Even
if GENERATE_MISSING is turned on, existing images may still be
used in case the name in the |
Preview images correspond to classes. The only possible setting is "OnClass=1". "OnVariant" must be set to '0'.
[STLIMPORT] OnClass=1
Preview images are displayed in the PARTdataManager in th directory tree and under Symbols/Details.
Note | |
---|---|
In this case the columns CLASSNAME and PREVIEWFILE are standard and must be filled out; the field MATNR must remain empty. |