Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Via the
Edit views command Preview, Technical drawings and 3D preview are assigned to either a
Class (= directory or project) or Variants of the class (= table
rows).
Class and Variants of the class are represented on the Edit views dialog via the tab pages.
The Edit views command is needed when you have added new classes (see Section 2.2.2, “ Add class ”) or new datasets (see Section 2.2.6, “ Add datasets ”) or want to change existing assignments.
In order to make changes proceed as follows:
Choose PARTdataManager Part selection when you want to make changes for a Class (directory or project).
Choose the Part view when you want to make changes for Variants of the class (table rows).
Call up the
Edit views dialog from the toolbar or from the context menu.
-> The same-named dialog opens.
Choose the desired files under Preview, Technical drawings and 3D preview via browse button .
The following tables exemplarily [9] show the relation between setting in the configuration file and dialog page.
Setting in
configuration file classimport.cfg
|
Area in the "Edit views" dialog |
[PREVIEWIMPORT] OnClass=1
|
|
[VIEWIMPORT] OnClass1=1 OnVariant1=0
|
Setting in the
configuration file classimport.cfg
|
Area in the "Edit views" dialog |
[STLIMPORT] OnVariant=1 OnClass=0
=> The setting is made on the Variants of the class tab page. |