Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following listing shows functions, which are needed for the article assignment.
You can search for the dimension of a variant or for a manufacturer article number, for example.
In the input
field, enter the desired term and click on the button Start text search .
-> Top right, under Line count, the total number of search results is displayed.
Furthermore you can search for any terms.
Text search settings: You can limit the text search to Search in links
or Search in
products. Click on the icon Text search settings
and in the dialog box, activate the desired
option (per default both are activated).
Filtering via attributes of product
assignments
Filtering is especially helpful if a long product list is displayed.
In order to filter you can use attributes such as Product filter, Quality, Type, Editing state or Affinity (see following figure). Based on the result you can then edit the remaining product links.
For this
click on the button Filter . -> The respective dialog box is
opened.
Select one of the following options:
When selecting this option the deactivated area with further options becomes activated.
Product filter -> Show products without links
If deactivated, then you can see products without links. At these products the small little arrow at the beginning of each line is missing.
Filter products by containing links
If activated, you can see products with links.
If the option is activated then further options are selectable under Quality, Type, Editing state and Affinity.
Type: There are two markups: D for Duplicate (unique assignment / 100%) and V for Variant.
Editing state: The attributes Valid or other (auto, default) can be activated.
Valid stands for products explicitly assigned via context menu command Change category to ... -> Valid.
deactivated: All products not explicitly set on Valid are displayed.
other (this includes auto and default) stands for products automatically assigned automatically (via pipeline) or manually.
deactivated: Only products explicitly set on Valid are displayed.
Example: Hide unique assignments
For this deactivate the checkbox Duplicate.
OpenAll: Click on
the icon in order to open or close the product table.
Refresh: Click on
the icon to be sure that a current result is displayed.