Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.5.2.2. Additional
information
2.5.2.2.2. Integration
of PARTsolutions CATIA interface in the CATIA environment
|
|
---|---|
Prev | Next |
The integration of the PARTsolutions interface in CATIA V5 is not executed automatically.
In order to have the PARTsolutions toolbar available in CATIA the interface has to be integrated in the CATIA environment. Proceed as follows:
Switch into
the PARTsolutions interface directory (e.g. $CADENAS/iface/catia/V5R2x
).
Depending on
the operation system variant either use the file "addenv-psc-32bit.txt
" or
"addenv-psc-64it.txt
" in
order to extend the CATIA environment.
Copy the complete content of the file at the end of your CATIA environment file.
The path
to your CATIA environment is found in the file "EnvDir.txt
".
For
example, this is found under "C:\Program
Files\Dassault Systemes\B21\win_b64
".
The path
is "C:\ProgramData\DassaultSystemes\CATEnv\CATIA.V5R20.B20.txt
"
for example. Possibly "ProgrammData" is not visible. If this is
the case then simply enter the path in the Explorer or set
"ProgrammData" visible.
Alternatively you can copy the content of
the file into a local environment to C:\Users\root\AppData\Roaming\DassaultSystemes\CATEnv
.
Further and current information is found in the file „readme.txt“. This file is stored with each PARTsolutions CATIA V5 interface in the installation directory.