Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the PARTsolutions menu of your CAD system click on Insert Connection. |
|
Choose the best elements for the definition of the distance. |
Per cursor you can capture corners, edges or parallel Layers (wall thicknesses) of the elements to be connected, as well as the Insertion point of the connection. Depending on whether you want to insert a through hole or a blind hole boring , you must determine the required reference plane on the surface of the selected elements.
-> The application switches to PARTdataManager.
Define the desired connection. More detailed information can be found here Section 3.1.1.10.4, “User interface in detail ”.
This option determines if the holes are exported as actual parts.
|
Then click on the button, or the menu command under Export -> Transfer to CAD.
The export of a Connection to your CAD system occurs analogously to the way parts and assemblies are transferred. See Abschnitt 3.1.1.11, „An CAD übertragen“.
-> The display quickly changes into the CAD system and the placement dialog opens. Choose the placement method by clicking on either "CAD system name" or on "In Cylinder". |
|
|