![]() |
In the Programs to start field, set the program that should be opened and the respective row content, if needed "continue processing". %DIR% pulls up the last transferred file, %NAME% takes over the name of that file. If the option Prompt for each file is activated, the program with every transferred row restarts every time, otherwise the launch takes place only once at the end of the batch.
In the Log file field you can apply a directory into which corresponding protocols can be entered in case of errors.