Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Make the settings on the below described AVI options and Cross-section tabbed pages:
Usually leave the default value "RGB32".
Otherwise select the desired bitmap format from the list field.
![]() |
Note |
---|---|
Please note the interaction of the settings under Rotation settings. If you set a rotation step to 1°, you will need 360 frames per rotation, so that a full rotation may be carried out. |
Delay between frames in 1/100 secs. (1-255)
The rotation speed is a result from this setting and the Animation frame setting.
You can adjust the color style to the layout of PARTsolutions versions, CAD systems and other style sheets:
8.1, 9.0, Purist, Metal, Wood, Catia V5, Solid Edge, SolidWorks, NX, One Space Designer, Pro/Engineer, Inventor
In order to get a transparent background, activate this option.
From the list field select the desired Codec.
The setting No Codec offers the best quality. However, without Codec you get very large files.
Select a Codec from the list with which the quality and file size are in the desired relationship.
Scale: Default value '1' (lowest possible value)
Time scaling. The larger the number, the slower the movement.
The more frames per second, the smoother the movement, but also the larger the file.
Usually you leave this setting. Changing to '2' would cut the number of key frames in half.
Optionally, you can define the rotational increment in degrees for individual axes.
Via Browse the Explorer opens.
If desired, change the path and the file name. Either way be sure to leave the file ending.