If colors have been used in catalogs for the part depiction, the Color Search can be used, either as only search method or in combination with other methods in order to enhance the result quality.
The Color Search contains two options: You can determine colors via color palette or load a picture, where the relevant colors are automatically scanned from. In the case of complicated dye distribution using an image file is advantageous.
Select the Colors tabbed page.
Select the desired color or color combination in the displayed list of the History section or select the desired color in the color range. (Multiple selection with Ctrl key).
If you
cannot find an appropriate color click on Add color and
determine the adequate color in the color picking dialog box.
Tolerance is in relation to the difference of RGB value (Red, Ggreen, Blue)
Example: When searching for the RGB value {230, 20, 20}, meaning a reddish color, with tolerance 10, the following colors are found.
220 <= R <= 240 and 10 <= G <= 30 and 10 <= B <= 30
Close dialog box Color Search by .
-> The search results are listed below.
In the Colors column and in the Part view the correct searched part color is displayed.
Select image for color comparison:
In the case of complicated dye distribution using an image file is advantageous.