![]() |
Sectional cuts are marked by hatches in the 2D preview. How these are changed for each part of an assembly can be configured via the following settings:
Possible hatch angles: 0.00,10.00,20.00,30.00
In the example, the first hatch angle is therefore 45° (+0°), the second 35° (-10°), the third 55° (+20°) and the fourth 25° (-30°).