Conflicts within the configuration are signalized by red highlighting of all affected parts.
In the following example, a conflict is caused due to a moving along the flute.
The cause are 2 crossing M12 write connections. These may not cross at the same position.
If the movement of the part is pushed all the way to the end position of "280" a conflict will arise.
Moving to end position "280" creates a conflict
M12 write connection
Conflict: everything marked in red