Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
3.1.6.8. Catalog, project
and part information
3.1.6.8.2. Docking window
Use Cases (Online)
|
|
---|---|
Prev | Next |
In the Part selection and in the Part view use cases from the knowledge database are displayed in an own docking Use Cases (Online).
Each use case is displayed exactly at that position (directory or project level) where it has been posted.
In the context menu of menus and toolbars you can find the item Use Cases (Online). Via checkbox you can set the visibility as desired.
With a click in the title and pressed mouse key you can move the docking (window) at the desired position. With a click on the pin you can enlarge the dialog. When you click on the pin in the opened state, then the dialog section is fixed.
When you select a directory or project which contains an use case, the number of use cases is displayed in red.
You can also participate yourself and post use cases. As soon you have registered the respective section is displayed. In order to register click on the respective link below.