Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
The exploded view can be opened via the toolbar or the menu.
The command is only active for assemblies.
The
Exploded view : ...shows the display of an assembly that has been
"drifted apart". Set the desired display criteria in the window
with the same name.
|
|
Animated : ...shows the drifting apart of the assembly components in a motion-sequence.
Rotate: ...rotates the assembly during explosion.
Not yet exploded transparent : To better differentiate, no transparents are yet displayed for drifted apart components.
Step 1 / ... model size: ... regulates the speed of the explosion.
![]() |
Note |
---|---|
The functions Rotate, Not yet exploded transparent and step 1/... model size can only be set once the option Animated has been activated. |
Reference lines : ...shows the relation between individual components via lines.
Automatic zoom : ...moves the part into the center of the window during explosion in order to obtain the largest possible display.