Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
If on the side of PARTsolutions the physical properties are set in the CNS classification, then these are also transferred to the CAD system during the export.
In PARTdataManager the attributes of the CNS classification are displayed under index tree, context menu of a part, menu item Part information.
In the following is explained how SolidWorks acts in different scenarios.
If a material has been transferred from PARTsolutions (material mapping), then this will always be applied and therefrom the density results.
The density detected via material has higher priority than an explicitly declaration of the density in form of an attribute.
If no material has been transferred from PARTsolutions, but an exact density from PARTsolutions, then the exact density is set.
If an exact mass is transferred from PARTsolutions, then the exact mass is set without the rest of the physical properties.
In the dialog box Mass properties then the option Assigned mass properties is activated.
The volume cannot be transferred from PARTsolutions, because it is calculated by the geometric model.