Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The exploded view can be opened via the toolbar or the menu.
The command is only active for assemblies.
The
Exploded view : ...shows the display of an assembly that has been
"drifted apart". Set the desired display criteria in the window
with the same name.
|
|
Animated : ...shows the drifting apart of the assembly components in a motion-sequence.
Rotate: ...rotates the assembly during explosion.
Not yet exploded transparent : To better differentiate, no transparents are yet displayed for drifted apart components.
Step 1 / ... model size: ... regulates the speed of the explosion.
Note | |
---|---|
The functions Rotate, Not yet exploded transparent and step 1/... model size can only be set once the option Animated has been activated. |
Reference lines : ...shows the relation between individual components via lines.
Automatic zoom : ...moves the part into the center of the window during explosion in order to obtain the largest possible display.