Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Now the registration is available for the desired version.
You get an error message, which says that the CAD system has to be started. However: It is already started.
The transfer could not be done!
You have to start the CAD system to create data
Probably the wrong version is registered.
You can check this by performing the following steps:
After this you receive the following output for example:
16.0.0.712 07/11/08 07:46:04 - Checking .NET Framework installation. Required version is: 2.0.50727 16.0.0.712 07/11/08 07:46:04 - Found the following .NET frameworks: v2.0.50727 16.0.0.712 07/11/08 07:46:04 - OK - Required .NET Framework version found: 2.0.50727 16.0.0.712 07/11/08 07:46:04 - .NET installation looks OK. 16.0.0.712 07/11/08 07:46:04 - Checking server object installation... 16.0.0.712 07/11/08 07:46:04 - Server object registration looks OK. 16.0.0.712 07/11/08 07:46:04 - Checking main interfaces... 16.0.0.712 07/11/08 07:46:04 - Interface\{5B45AFF1-D3B8-4e0d-BB90-B1DF834AEC1D}\ : ERROR - Cannot find registry entryFe 16.0.0.712 07/11/08 07:46:04 - *** Main interfaces problem detected. 16.0.0.712 07/11/08 07:46:04 - Checking type library registration... 16.0.0.712 07/11/08 07:46:04 - Type library registration looks OK. 16.0.0.712 07/11/08 07:46:04 - Checking application object registration... 16.0.0.712 07/11/08 07:46:04 - CLSID\{00E6D1B8-0F10-4ab8-A98A-5F413D9A9E8C}\: ERROR - Cannot find registry entry 16.0.0.712 07/11/08 07:46:04 - *** Application object registration problem detected. 16.0.0.712 07/11/08 07:46:04 - Checking download cache... 16.0.0.712 07/11/08 07:46:04 - Download cache looks OK. 16.0.0.712 07/11/08 07:46:04 - Checking GAC... 16.0.0.712 07/11/08 07:46:04 - GAC looks OK.
The output shows that there is an error at the registration.
In order to solve the problem please start the desired Modeling version from the console with the following command:
..\SolidDesinger.exe -register
Check the registration of the components once again via (f2::check-api-installation).
16.0.0.712 07/11/08 09:54:03 - Checking .NET Framework installation. Required version is: 2.0.50727 16.0.0.712 07/11/08 09:54:03 - Found the following .NET frameworks: v2.0.50727 16.0.0.712 07/11/08 09:54:03 - OK - Required .NET Framework version found: 2.0.50727 16.0.0.712 07/11/08 09:54:03 - .NET installation looks OK. 16.0.0.712 07/11/08 09:54:03 - Checking server object installation... 16.0.0.712 07/11/08 09:54:03 - Server object registration looks OK. 16.0.0.712 07/11/08 09:54:03 - Checking main interfaces... 16.0.0.712 07/11/08 09:54:03 - Main interfaces registration looks OK. 16.0.0.712 07/11/08 09:54:03 - Checking type library registration... 16.0.0.712 07/11/08 09:54:03 - Type library registration looks OK. 16.0.0.712 07/11/08 09:54:03 - Checking application object registration... 16.0.0.712 07/11/08 09:54:03 - Application object registration looks OK. 16.0.0.712 07/11/08 09:54:03 - Checking download cache... 16.0.0.712 07/11/08 09:54:03 - Download cache looks OK. 16.0.0.712 07/11/08 09:54:03 - Checking GAC... 16.0.0.712 07/11/08 09:54:03 - GAC looks OK.