powered by CADENAS

Manual

Manual

5.21.7.7.3. Column sorting of geometry columns in PARTdataManager

In order to change the column sorting (for the current project), proceed as follows:

  1. PARTlinkManager -> Extras menu -> Database -> Edit additional tables

    Click on the menu item Edit additional tables. -> The Edit table dialog box opens.

  2. In the list field under Select table select "PRJTABLE".

  3. In the column PRJ_PATH enter the project path, in the column VKEY the value COLUMN_SORT and in the column VVALUE the geometric columns to be displayed in the front position. In the following exemplary figure these are the columns D, L, and P.

  4. Now start PARTdataManager.

    The desired columns are displayed in the front (in the given sequence).

VKEY: COLUMN_SORT

VKEY: COLUMN_SORT

[Note] Note

Related subjects:

  • Column sorting of ERP columns

  • Geometry columns at a certain position between the ERP columns.

See Section 5.11.1, “ Tabbed page "General" ” -> Column visibility.