powered by CADENAS

Manual

Manual

2.3.8. SpaceClaim - Administration

The following integration description is valid as of SpaceClaim Engineer version 2012 and PARTsolutions as of 9.07

Installation

In order to install the SpaceClaim interface proceed as follows:

  1. In the installation routine select the interface.

    After successful installation you can find the interface under ../Programs(x86)/SpaceClaim/Addins/PartSolutions\ifspcl2012_32.xml.

  2. The path in the parameter „assembly“ should already be correct.

    <?xml version="1.0" encoding="utf-8" ?>
    <AddIns>
      <AddIn
        name="CADENAS PARTsolutions V9"
        description="CADENAS PARTsolutions V9 Integration for SpaceClaim 2012 32Bit"
        assembly="F:\psol90\software\iface\spaceclaim\2012_32\ifspcl2012_32.dll"
        typename="Cadenas.PartSolutions.SpaceClaimFullAddinNet"
        host="SameAppDomain" />
    </AddIns>

Now the interface is operative.

User documentation

The corresponding user documentation is found under: