Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.3.6.2. Attribute
mapping in Solid Edge
2.3.6.2.6. Set different
languages for attributes
|
|
---|---|
Prev | Next |
The language set on the tabbed page AttributeMapping(3D) under Attr_CopyFrom_01 is valid for all PARTsolutions standard attributes.
Note | |
---|---|
If there is no translation for the language of the attribute, no attribute is exported (not even from $CADENAS_LANGUAGE language). |
Optionally for each individual extra attribute a specific language may be assigned. In this example "LINA".
The setting must be made via PARTadmin -> Category -> PARTsolutions -> Configuration file -> $CADENAS_SETUP directly in the configuration file.
?GetObject("iface.calcnameservice").start(0).Format("<ATTR(english,LINA)>").value()
The display occurs after restarting PARTadmin on the tabbed page Custom in this form:
Display text of modified configuration file on tabbed page, depending on whether or not language was specified explicitly
Note | |
---|---|
All attributes which were not assigned an explicit language, will be exported in the set $CADENAS_LANGUAGE language. In this example "NT". |
Result: Attributes in Solid Edge under File properties -> tabbed page Use-defined:
French edition for standard attributes (tabbed page "AttributeMapping(3D"); German for the user-defined attributes (tabbed page "Custom" )and English for the user-define attributes with explicit language specification (special entry in configuration file)