powered by CADENAS

Manual

Manual

1.1.7.4.3.1. General settings
Section COMMON

The section COMMON concerns general settings.

  • ACTIVE = (Value range 0 or 1)

    Feature active; yes or no.

  • SHOWBITMAPS = (Value range 0 or 1)

    In the selection window of the PARTdataManager a Bitmap is displayed / yes or no.

  • USE_LINKDB = (Value range 0 or 1)

    For large amounts of data, you have the option to manage the replacement files in a separate table "REPLACE_TABLE". This is activated with "1". The replacement files are either taken from the configuration file or the REPLACE_TABLE.

    See also Section 5.2.3.3, “Additional functionalities ”.

  • LINKDB_TABLENAME=replace_table

    Optionally, the name of the replacement table can be shown.

  • TREEICONS = (Value range 0 or 1)

    Value = 1: Replaced or crossed out without replacement standards are identified by a symbol in the directory tree of the PARTdataManager.

Section COMMON(Role1)

In the COMMON(Role1) section, the replacement table can only be activated for certain roles or users.

  • ACTIVE = (Value range 0 or 1)