Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.1.1. User
interface for Category "CAD integration"
2.1.1.3. Mode:
"Simple" or "Expanded"
|
|
---|---|
Prev | Next |
For some keys there are two modes possible for the display of key values.
When you right-click on a value name Expand or Simplify is displayed. With these two commands you can switch between the modes.
If both modes are possible the default is the simple mode.
The advantage in this mode is to only display relevant, changeable sections of the key.
This way you can define single values such as file extension or a variable.
Often specific parameters are embedded in complex VB expressions so that very complex changes and adjustments can be made. However therefor exact knowledge of the Syntax is necessary. For such changes use the expanded mode.
?GetObject("iface.calcnameservice").start(0).Format("<GENNAME><MATERIAL(_)>") .toFileName("_").add(".ipt").value()
Here the file extension could be adjusted, for the file name allowed characters could be defined, upper-case characters could be changed into lower-case characters. You can find detailed information under Section 2.2.1.4, “Variable values - functions ”.