Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.3.3.
CoCreate Modeling Integration - Administration
2.3.3.4.
Block
[AttributeMapping(is3d)]
|
|
---|---|
Prev | Next |
PARTsolutions variables (geometric, NT, NN, LINA, etc.) and all fields in the link database (if an ERP connection exists) can be transferred to CoCreate Modelling or Creo Elements/Direct Modeling via attribute mapping.
Attribute mapping is controlled by the following blocks:
In the block [AttributeMapping(is3d)] you determine whether the PARTsolutions standard attributes (geometric, NT, NN, LINA, etc.) are to be exported to the CAD system and if so, in which language(s).
Under Attr_CopyFrom_01 set the desired language. The keys Attr_Content_01 and Attr_Section_01 remain unchanged.
default: The attributes are exported in English.
Assign language: The standard attributes are exported in the indicated language.
default, german,english, italian, french, spanish, portuguese, czech, slovak, hungarian, slovenian, dutch, danish, finnish, russian, japanese, korean, chinese, polish
Note | |
---|---|
If there is no translation for the indicated language of the attribute, no attribute is exported (not even from the german language). |
No entry: No standard attributes are exported. (In order to explicitly export specific attributes, use the other sections.