Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order that the material mapping can be executed, so that in Creo/ProEngineer the correct material is displayed at a part transferred from PARTsolutions, the respective settings have to be performed:
Configuration file settings concern ...
the material selection in PARTdataManager (the material value displayed in the column "MAT_NAME" [also see Section 2.2.5, “Material mapping ”])
Per default the
material is displayed in the table column MAT_NAME
when an ERP integration
is available.
Depending on the
company-internal workflow the material can be set (together with an
ERP_PDM_NUMBER
)
directly in PARTdataManager for
example.
The procedure in PARTdataManager is as follows:
Open the list
field under Material. Exactly
those materials are displayed, which are set in the configuration file
$CADENAS_SETUP/material_assign.cfg
.
Detailed information on material mapping can be found under Section 2.2.5, “Material
mapping
”.
Select a material and confirm with .
-> At the selected characteristic, which is to be exported, now the desired material is displayed. (In this exemplary procedure the ERP number has been automatically generated.)
At Creo/ProE the
material files are stored under C:\Program Files\PTC\Creo 1.0\Common
Files\M020\text\materials-library
.
In a first step,
under block Interface,
key MaterialDirectories
, determine
the path to the material library in Creo/ProE.
This can either be the standard path or any path. Should there be more than one material library, then enter the paths comma separated.
Tip | |
---|---|
It's easy to find a key. Simply call up the dialog box Searching... via context menu command Search key (over any configuration file). Determine the search options and click on .
|
In a second step determine the mapping in the MatMAP section. Key value is the name of the respective mtl file. Lower or upper case doesn't matter.
Apply exactly
those keys, which are set in the configuration file material_assign.cfg
or can be a
value in the column MAT_NAME.
So in this example apply the key "STEEL" among others.
Key value is the name of the respective mtl file.
Now the corresponding material properties are also used for PARTsolutions parts.