Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
The
configuration file |
In this file you can specify the ODBC or JDBC database interface for each used operating system.
The driver
selection during the PARTsolutions setup (Database connection selection) results in a
setting in dbproxy.cfg
.
If for testing purposes or by mistake a wrong driver has been selected, set the correct driver in the configuration file or in the corresponding user interface.
Under PARTadmin -> category PARTsolutions -> ERP environment, in the Database interface dialog area, you can make settings easily via user interface:
Either you determine ODBC or JDBC specifically for each operating system. Or you determine the default interface and then refer to the selection <default> in the list field.
Setting via configuration file:
[COMMON] Driver=DATABASE.ODBCDB [x86] Driver=DATABASE.JDBCDB [Linux] Driver=DATABASE.ODBCDB [AIX] Driver=DATABASE.JDBCDB
Either you determine ODBC or JDBC specifically for each operating system or the one specified in the block [Common] is taken.