Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the
configuration file replace_std.cfg
replacement
projects can be specified.
Example: DIN 912 is replaced by ISO 4762.
norm/ din_en_iso/ schrauben/ zylinderschrauben/ din_en_iso_4762.prj |
||
Further projects to be listed can be stated. These are incremented with NEWx. |
||
After an
update from V8 to
V9 it can be the case, that the path statements in
the configuration file are not correctly anymore. Then the script file migrate_replace_std_v8_v9.vbb
can
be used, in order to adjust the paths in the configuration file replace_std.cfg
.
Field of application for the script
The script can be used in customization projects, where own standard catalogs are used.
The script reads
in the old replace_std.cfg
and compares the
entries with the current catalog status, in order to check, whether the
paths under SECTION and under VALUE are correctly for each line
SECTION-NEW1, SECTION-NEW2, etc.
If not, then it is searched for the
project names. According to the found correct paths a new configuration file
replace_std_updated.cfg
is created.
Furthermore a log
file replace_std_updated.log
is
created. It contains a respective entry for each line:
The .log file is configured as tabstop separated CSV file and contains the columns "status", "old" and "new".
The following values for the column "status" are possible:
After the script has finished, you can check with the help of the log file, which paths have not been found, etc.
The script is not available in the installation. If needed please contact the CADENAS Consulting team.
Also see Section 1.7.3.3, “ replace_std.cfg ”.