Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If in an update version a directory, project or certain characteristic is missing, then it can be the case that LinkDB links have no target.
As soon as a certain characteristic is selected in the index tree, you can recognize on the right side, in the section Line mapping as well that there is no assignment:
A missing automatic assignment of a project does not necessarily mean, that it does not exist; it could be that only the name has been changed.
For editing of assignments you have two options:
You can confirm the missing assignment now in the section Line mapping in the column New dataset via click on the green checkmark .
Now there are two further cases:
A new line assignment shall be made in the same project.
-> Hereto change the line selection in the table and confirm with the command Approve assignment.
A new line assignment shall be made in another project.
By clicking on the button Search project the dialog box Search opens on the tabbed page Search.
Perform a text or variable search.
By double-clicking on one of the search results the desired part is assigned.
Alternatively you can switch to the Choose tabbed page and there browse to the desired part/project. Then you can load the project via double-click into the column New dataset. Now select the desired characteristic.
Regardless of the chosen variant now finally confirm the new assignment by clicking on the green checkmark Approve assignment.
Now the symbol for an assigned and approved dataset is displayed in the index tree, in the respective line. |
|