Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
2.3.1.3.
Attribute mapping in AutoCAD
2.3.1.3.3. Block
[BomNormalAttributes] - Define BOM list attributes
|
|
---|---|
Prev | Next |
In the block BomNormalAttributes you determine which PARTsolutions attributes are to be exported to the BOM list.
Optionally you may also change the field entries or insert text or variables into empty ones.
Per Default only the attributes "Description", "Standard" and "Material" are displayed in the BOM list (BOM list table) in AutoCAD.
If you add columns to the BOM list window, you can see which other attributes were exported from PARTsolutions in the window Select columns (compare to fig. ???). As soon as you have inserted the columns, these are made visible with the PARTsolutions export value.
BOM list table with the desired columns inserted into the drawing: