Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
![]() |
Note |
---|---|
The standard declaration is normally completely sufficient. For the sake of completeness, it shall be mentioned that the ERP material column can also be specified directly. |
There are two possibilities: Without and with mapping table.
The material name is directly taken from the ERP material column (default is "MAT_NAME") and transferred 1:1.
The mapping table is not used.
?GetObject("iface.calcnameservice").start(0).Format("<ATTR(MAT_NAME)>").value()
The material name is directly taken from the ERP material column (default is "MAT_NAME").
Then, with the help of the mapping table (see Configuration File -> Block "MatMap"), the determined name is mapped onto the CAD system material name.
?context.TranslateStringInGlobalOptionArray("MATMAP","",GetObject("iface.calcnameservice").start(0).Format("<ATTR(MAT_NAME)>").value())