Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Determine ODBC or JDBC database interface for each operating system. Under PARTadmin -> Category PARTsolutions -> ERP environment, in the Database interface dialog area you can make settings easily via user interface:
If there is no specific entry available, the entry under [Common] (Default) is used.
This configuration file is only available if a link database with the required driver is used.
[COMMON] Driver=DATABASE.ODBCDB [x86] Driver=DATABASE.JDBCDB [Linux] Driver=DATABASE.ODBCDB [AIX] Driver=DATABASE.JDBCDB
Either you determine ODBC or JDBC specifically for each operating system. Or you determine the default interface and then refer to the selection <default> in the list field.