Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For connection elements such as screws, nuts, rings, pins, etc.m the cutting in the 2D view may be excluded.
Default settings
are made in the CAD spanning configuration file ifacecommon.cfg
, in the block
[CreationOptions], in the key "NoSection".
For any changes use the same key in the CAD specific configuration file.
Note | |
---|---|
The exact same key overwrites the default setting in ifacecommon.cfg; information of different keys is merged. |
In image 1 below you can see that with activation of the function only the plate is cut and not the screw itself.
The default setting in the section [CreationOptions] is:
[CreationOptions] NoSection(is3dPart)=?(GetObject("iface.metaoptionservice").GetObj().PartAttr. IgnoreSectionViewCut) or (context.IsStringInGlobalOptionArray("NoSection","nosection_", Replace(GetObject("iface.metaoptionservice").GetObj().mident, "/", "\\")))
The default setting in the section [NoSection] is:
[NoSection] nosection_0=norm\din\schrauben nosection_1=norm\din\muttern nosection_2=norm\din\zubehoer\ringe nosection_4=norm\din\zubehoer\scheiben nosection_5=norm\iso\schrauben nosection_6=norm\iso\muttern nosection_7=norm\iso\zubehoer\ringe etc.