Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the key
VisibleSearchPages
, you
can specify the search methods to be shown. This key is inactive by
default.
Enter the desired search methods separated by comma. At first possibly activate the key.
[SettingsSearch] VisibleSearchPages=KeySearch,VarSearch,GeomSearch3D,GeomSearch2D,ColorSearch,TopoSearch, RawPartSearch
Full-text search and Variables search are always available by default. The other search methods require the license "CNS200x*PSADDONS*COMPLEXSEARCH.
When, using the Geometric search (3D), the number of displayed search results is lower than the set maximal number due to the requested Minimum similarity, then at the end of the list of search results the button Extend search range to xy% similarity is displayed.
In this figure the button shows the value "Extend search range to 80% similarity". The default value for minimum similarity has been 90%. Using standard settings the percent value is reduced by 10 percent points per click and the search is started again.
The percent
value of step range to reduce the minimum similarity is set to 10 by
default. If you want to change the value, then create the two following keys
in PARTadmin under
$CADENAS_USER/psolopt.cfg
.
If you want to change the standard, then set the two following keys:
[SettingsSearch] GeoSearchHintStepSize=10 GeoSearchHintMinValue=50
The first key determines the step range, the second key sets the lowest minimum similarity.