Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Settings for part selection in PARTdataManager:
In the standard catalog, for example, fingerprints only exist for a few lines. Now, when setting the option Topology values, the generation of missing topology data is processed by default.
If this is not wanted, set the following:
[SettingsIndexTree] GenerateMissingTopologyData=0
Set the above key with value 0.
You can configure, whether the variables and their values shall be clickable in search results.
When clicking on a variable a variable search is directly performed, value based on it.
When clicking on a variable the dialog box Variables search opens.
[SettingsIndexTree] ClickableVariables=1 (Default)
If filters such as Preferred rows on/off are enabled, this affects (reduces) the search results. Compare Section 3.1.2.7.2.3, “ Use preferred rows filter ” in PARTsolutions / PARTcommunity4Enterprise - User manual.
Via key SearchFilterHint_MaxResults
you
can adjust, whether a respective message is displayed at all or which number
of hits is displayed below.
"Note: preferred rows are enabled! You only get hits from projects with at least one ERP assignment. The number of hits increases likely, if you disable it in the toolbar."
[SettingsIndexTree] SearchFilterHint_MaxResults=
At all search methods the placement number is displayed in the first column.
The placement number can be displayed or hidden via configuration file.
Configuration file: psolopt.cfg
[SettingsIndexTree] ShowDisplayRanking=0/1
1: Placement number on (default)
In the following cases additional information is found in the popup window:
Topology search with "Any parameter" delivers a lot of values. In order for all values to be displayed, click into the cell.
If the following key is not available, then you may add it yourself.
[SettingsIndexTree} EnableOverlayPopup=0
Relation: PARTdataManager -> Dialog area Links -> displayed options in the list field
Adjust the comma separated values as desired.
PARTdataManager -> Context menu of any toolbar or menu bar
Indicates whether the dock Use Cases (Online) should be shown.
[SettingsIndexTree] SHOWUSECASESDOCK=1
If Use Cases (Online) is principally activated, nevertheless the user can decide, whether the feature shall be active or not.
Using PARTsynonym you can define and manage synonyms.
Among other things, the synonyms you defined can be taken into account in PARTdataManager during the Full-text search.
This way you can find products, you otherwise wouldn't have found by reason of different notation (e.g. hexagon screw, hexagon head screw, hexagon head set screw, hexagon bolt, ...).
In PARTadmin, in order to enter data click on Start PARTsynonym!.
In PARTdataManager, check/uncheck the option in order to use the search database.
[SettingsIndexTree] KeySynonyms=
-1=disabled: The Search for synonyms pushbutton is not shown in the PARTdataManager.
More information about the synonym editor can be found under Section 1.1.8, “ PARTsynonym ”.