Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For the attribute mapping you can group the single attributes in categories and optionally assign an attribute type.
Perform the settings as follows:
At first, in the block [CadDocumentAttributes], the attribute is created with the desired value. The value can be fixed or be specified using an expression such as "?_ATTR("NB")" for example.
[CadDocumentAttributes] TestAttribute=42 TestAttribute.custom=Category.TestCategory, Type.Integer TestAttribute2=1 TestAttribute2.custom=Category.TestCategory, Type.number
Then the desired category is created using the following syntax.
CREATOR.custom=Category.Testcategory
Optionally, after the category, the attribute type can be specified separated by comma. If no type is specified, the type will be "String" by default.
The following "custom" type values are supported (string is "default"):
CREATOR.custom=Category.Testcategory, Type.Integer
After export the attribute is found in NX under "Component Properties" in the applied category "TestCategory".