Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
When changing the default configuration all changes are written in a second Setup directory. In this way it is directly evident, whether changes have been made at all and if so in which scope and which exactly. The Default_User directory is also inside this Setup and will be managed as well.
In order to activate the function specify an environment variable CADENAS_SITESETUP in the start.env (the directory has already to be existent). For example:
CADENAS_SITESETUP=$CADENAS/sitesetup
If the function is active and any PARTsolutions application attempts to write into SETUP, then all changes are automatically saved and displayed under SITESETUP. When a changed value is set on the default again, then the entry is automatically removed from the SiteSetup.
Via "Conditions"
you can easily specify conditional sections in the start.env
for your installation
and so use different Setup directories. On this please see ???.
An existing second Setup is also displayed in PARTadmin beside the default Setup.