Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Many standard functions, such as for example adjusting a variable or setting a numerical value, can be best carried out under the Category CAD integration.
In the case of complex changes it is wise to edit directly in the configuration file.
However therefor detailed knowledge of Syntax is necessary. Changes should only be made by experienced users or consultants here.[33]
During
interpretation of settings, the CAD specific (ifsolidworks.cfg
, ifacad.cfg
, etc.) and the
general configuration file (ifacecommon.cfg
) are
used.
The figure shows the Category "Configuration files" using to the selection "$CADENAS_SETUP -> if<cadname>.cfg"
[33] The CAD and PDM interfaces of PARTsolutions exhibit a high flexibility due to the scripting option. The programming language used here is Visual Basic. Through a CADENAS own script interpreter the scripts work both under Windows as well as under Unix.