Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the block AttributeMapping(is3d) you can define whether the PARTsolutions standard attributes are to be exported to the CAD system and if so, in which language(s).
Under Attr_CopyFrom_00 bis ...0x set the desired languages. The keys Attr_Content_00 bis ...0x and Attr_Section_00 bis 0x remain unchanged.
default: The attributes are exported in $CADENAS_LANGUAGE.
Attr_CopyFrom_00=default,var_visible=1
In order to differentiate the parameters var_exclude and var_visible can be used.
Possible values are: default, german, english, italian, french, spanish, portuguese, czech, slovak, hungarian, slovenian, dutch, danish, finnish, russian, japanese, korean, chinese, polish
The standard attributes are transferred in the set language.
Note | |
---|---|
If there is no translation for an attribute in the selected language, no attribute is exported (not even from the $CADENAS_LANGUAGE language). |
No entry: If you leave all Attr_CopyFrom fields blank, no standard attributes will be exported.
In order to explicitly transfer special attributes please use the block [CadDocumentAttributes].
Optionally, you can determine a prefix for each language via keys Attr_Prefix_0x. In this way the standard attributes can be differentiated between each other in the list of the dialog box Parameter.
Detailed information on attribute mapping can be found under Section 2.2.4, “Attribute mapping ”.