Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The configuration file erpcustom.cfg
is used in order to
customize ERP processing.
Some functions are called up via ERP toolbar.
The file is subdivided in a couple of blocks which are explained in the following.
The blocks USERDIALOG, VARS, LOAD, BEFTBLLOAD, AFTTBLLOAD, MAIL, ADDTODB may be applied role-specific according to the scheme of Block(Role).
The "DESCRIPTION" field might be important for the administrator during the application of data. So incorporate the field USERDIALOG for the "Administrator" role.
The "DESCRIPTION" field is probably unimportant for a designer when applying for a part per e-mail. So do not incorporate it in the MAIL dialog for the "Designer" role.
When using the SAP MM interface also see Section 3.3.8.11, “Customizing the PARTsolutions ERP interface”.