Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
In the course of part export to the CAD system the material attribute plays an important role. The aim is that the physical properties can be calculated and assigned in the CAD with the help of the transferred attribute.
The standard procedure is the following:
PARTadmin -> Category -> Configuration files -> $CADENAS_SETUP -> if<cadname>.cfg -> Block CreationOptions(is3d) -> Key Material
The key "Material" defines, that the material name is fetched according to the definition in the CNS classification.
Material=?context.TranslateStringInGlobalOptionArray("MATMAP","",_FORMAT_0("<CLASSPROP(cns,CNSPHYPROP,CNSMAT)>").value())
When using an ERP integration the material is taken from the column MAT_NAME by default, without ERP integration from the column CNSMAT.
The determined name is then mapped with the help of the mapping table (PARTadmin -> Category Configuration files -> $CADENAS_SETUP ->if<cadname>.cfg -> Block MatMap) to the CAD system material name.
If the block "MatMap" or needed materials should be missing, then simply set them yourself. Information on this can be found under Section 1.1.6.3, “ Configuration files functions ”.
Where the CNS
classification gets the material name from, is set under $CADENAS_SETUP
-> configuration file ifacecommon.cfg
-> Block
[ClassMapping].