Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Definition der Verschraubungstypen:
Die Schlüssel "Unit", "Hole" und "Counterbore" gehören zu den Verschraubungstyp-Filtern (Default).
Definition of the connection types:
The keys "Unit", "Hole" and "Counterbore" are part of the connection type filters (default).
Always show holes (without ERP integration as well) regardless whether button "Preferred rows on/off" is activated or not.
Normally holes are not managed via ERP. Meaning that these are "red" and thus are hidden when (Preferred rows on/off) is on.
Because this behavior normally is not desired, all classes of holes are explicitly specified in the key "ClassIdsSkipErp" and thus exclude from filtering.
Note | |
---|---|
The
setting has to be performed in the configuration file under
|
[ThroughHole:ThreadNutside:CommonOuterdrive]
ClassIdsBoltside=HOLES_COMMON_THROUGHHOLE,WASHER,LOCKWASHER,BOLTS_COMMON_OUTERDRIVE
...
ClassIdsSkipErp=HOLES_COMMON_THROUGHHOLE,HOLES_COMMON_THROUGHHOLETHREAD
...
...
Result in Connection dialog area: