Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
It is recommended to use the 64-Bit variant of PARTadmin, because the conversion is much quicker in this way, because more working memory is available.
The Standards catalog can only be migrated as a whole. It is not possible to only migrate "norm/din" for example.
You can migrate several catalogs at once.
You have updated PARTsolutions V9 from version <= 9.07 to version >= 9.08.
Open PARTadmin -> Category -> PARTsolutions -> Catalog update -> Migration.
-> Now all catalogs are displayed in the dialog section Available catalogs.
Mark the checkbox for those catalogs to be migrated. (For example in the image above, BikeCompany.)
--> The display automatically changes to the Migration tabbed page.
This is where the migration process is protocolled. At the end you are informed whether the migration was conducted successfully.
Switch back to the Catalog list tabbed page and click on Refresh list.
--> The
migrated catalog (exemplified here by "BikeCompany") now shows the
icon Geometrical index existing (new V9 index) in the column V9V2.