Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
During assembly export from PARTsolutions to Autodesk Inventor, an inquiry is sent to the PDM (Vault): Is the corresponding part already stored in the database or not?
If yes, the part is read from the PDM and copied into the inventor working directory on the local computer (Vault Operation "DownloadFile"). This local copy is then sent to the CAD.
If not, the corresponding part will be created in the PARTsolutions parts pool. After this generation it will be "checked into" VAULT.
The Vault Interface was carried out under use of the Apache AXIS 1.3 JAX-RPC implementation. Technically, the following overall architecture is given:
All requests go directly to the Autodesk Data Management Server. An installed Vault Client is basically not needed. The necessary infrastructure (CADENAS vbs, Java VM) is an inherent art in PARTsolutions and available independent of the operating system.