Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.2.2.3. Reuse the
V8.1 pools after migration to V9
2.2.2.3.1. File name
with reuse of V8.1 pool
|
|
---|---|
Prev | Next |
The file name shall be the same just as in version 8.1. This enables to reuse a part from v8.1 pool which has been created under v8.1.
Important | |
---|---|
Make sure with V10 setting methods that the file name is the same just as in V8.1. The file name is set by the FileName key. Be oriented towards the examples under Section 2.2.2.2, “File name: set generation options ("FileName" key) ”. |
Example by reference to Inventor:
With the default setting in V8.1 the file name was created with underscores.
Cylinder_head_screw_ISO_4762_M20x90.ipt
On the base of the default setting in V9 you have to replace toFileName("_") with alnum("_") in order to create the file name in the same way such as under V8.1.