Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
INSERTS, DELETES and manual UPDATES (by PARTlinkManager or PARTdataManager) are automatically logged in the table LOGTABLE.
LOGID VARCHAR(40) NOT NULL, TABNAME VARCHAR(15) NOT NULL, KEYFLD VARCHAR(15) NOT NULL, LOGKEY VARCHAR(500) NOT NULL, LOGEXT VARCHAR(64), LOGTIME VARCHAR(20) NOT NULL, USERNAME NVARCHAR(20), HOSTNAME NVARCHAR(20), PROGNAME VARCHAR(15), MODTYPE SMALLINT DEFAULT 0 NOT NULL, UPDSEARCH SMALLINT DEFAULT 0 NOT NULL,
You can view this table via PARTlinkManager -> Extras menu -> Database -> Edit additional tables.
Meaning of single LOGTABLE columns
In order for the
task to be performed the following settings have to be made in the
configuration file pappserver.cfg
.
[TaskManagerModule] TimerInterval=60 tasks=loadAll DBSearchIndexTask=1h DBClearLogTask=24h [DBClearLogTask] DaysToKeep=365
TimerInterval: Specification in which interval (seconds) it shall be checked whether a new task is pending. Normally this does not have to be adjusted.
DBSearchIndexTask: Task interval for updating the ERP search index. The task checks the LOGTABLE whether there are new entries available. If yes, the ERP search index is updated.
DBClearLogTask: Task interval for clearing the LOGTABLE. This task deletes all entries from LOGTABLE.
1m | Task is executed every minute |
1h | Task is executed every hour |
13:21z | Task is executed every day at 13:21 GMT |
mon 14:30 | Task is executed every Monday at 14:30 (locale time) |
DaysToKeep: Number of days to store the entries in the LOGTABLE.