Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If the performance at secondary locations should be improved (especially with large assemblies/ZJVs) you can use RFS or SQUID.[64]
For external access from PARTsolutions to the PARTapplicationServer from secondary locations SQUID can be optionally installed. Squid is free software, which is installed at customer site.
Squid is a proxy for caching, which supports HTTP, among others. Squid optimizes the data flow between client and server and caches often used data (especially project and ZJV files). At large assemblies (also at native parts) the use of SQUID can improve the performance. Everything which has ever been loaded is in the local cache. In order to make sure that all files are always up-to-date, Squid checks this at each access.
If using Squid would mean a disproportionate effort or is not necessary for performance reasons, RFS Caching can be an alternative. RFS works with UNC and therefore is a bit slower than HTTP+Squid.
Activation: Under %CADENAS_SETUP%/partsol.cfg
-> block [RemoteFileSystem]
->
key CacheActive
set the value to 1.
[RemoteFileSystem] CacheActive= 0 or 1 CacheDir=$CADENAS_USER/rfs CacheSize=50
CacheDir can be an UNC path wherewith you can realize a common caching.
![]() |
Note |
---|---|
The cache can be initially filled via VBS scripting for certain catalogs. And via VBS command the files are nightly grabbed and copied in a temp-directory. Thereby the cache is filled. |
![]() |
Note |
---|---|
A diagram for distinction of different caching methods can be found under Section 4.5.3, “Caching methods for data storage and operation ”. |