Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
4.24.5.6. Tabbed pages
Standard name , Standard name (short) , BOM name
4.24.5.6.2. Examples
|
|
---|---|
Prev | Next |
If there is no explicit intervention at the Standard name tab page, then the name is automatically created with the NB (Standard name).
The entry NB=$NB would be appropriate.
Example 2: A condition is used.
If there is no ERP number available then the NB (Standard name) is created by default. Otherwise the ERP number is used.
Through the ERP_PDM_NUMBER uniqueness is ensured. The standard name provides a meaningful part in the file name.
IF ('$ERP_PDM_NUMBER.'.EQ.'')THEN NB = '$NB.' ELSE NB = '$ERP_PDM_NUMBER._$NB' ENDIF
Example 3: The project version is suffixed to the Standard name.
If there are different strength, surfaces, etc. available for parts which are identic regarding their geometry then this can be considered in the naming rule.
e.g.: Creation of the file name by NB plus material.
![]() |
Note |
---|---|
Names assembled in this way can quickly call up an exceeding number of maximally allowed symbols. |
Creation of the file name by the ERP_PDM_NUMBER.
Combination of ERP_PDM_NUMBER and "SHORTNB"
NB=(’$ERP_PDM_NUMBER._$SHORTNB.’)
IF ('$ERP_PDM_NUMBER.'.EQ.'')THEN
Meaning: In case an ERP_PDM_NUMBER exists, the standard NB is used, otherwise the ERP_PDM_NUMBER + NB.