Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The AppServer knows all changes to the database so that it can react with updates of the LinkDB search index or client notifications at project changes and/or role changes.
If the option Catalog browsing and search with AppServer is chosen (meaning not Catalog browsing, search and database with AppServer automatic updates of the LinkDB search index work anyway. This is possible, because a "Task" can be configured on the AppServer, which continuously updates the LinkDB search index (with the help of LOGTABLE information).
An older
concept (up to V9.08) is using the script nightupdate_erp.vbb
for index
updates. It ensures that the ERPTABLE is integrated into the full-text
search index (=Lucene index). (Optionally, can also be used in V10.)
(Details can be found in the script itself.) The advantage of the
AppServer solution is that only those parts of the LinkDB search index
are updated, where data has been changed. If there are no special causes
the nightupdate_erp.vbb
is not
needed in V10 anymore.
Task interval for updating the ERP search index. The Task checks the LOGTABLE whether there are new entries available. If yes, the ERP search index is updated
If the value is set, then after a catalog update the search index is automatically updated.
If you do not want an automatism at this place, but initiate it manually, then do the following:
On this also see Section 4.17.9, “ Update full-text search index / plinkcommon.cfg -> Block [Common] -> Key "UPDATESEARCHINDEX" ”.
DBClearLogTask: Task interval for clearing the LOGTABLE. This Task deletes all entries from LOGTABLE.