Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
When changing the default configuration all changes are written in a second Setup directory. In this way it is directly evident, whether changes have been made at all and if so in which scope and which exactly. The Default_User directory is also inside this Setup and will be managed as well.
In order to
activate the function specify an environment variable CADENAS_SITESETUP
(e.g. in the start.env
). The directory has
already to be existent. For example:
CADENAS_SITESETUP=$CADENAS/sitesetup
If the function is active and any PARTsolutions application attempts to write into SETUP, then a copy of the respective configuration file is automatically created under SITESETUP and the changes are saved there. If the default is restored, the respective file is deleted under SITESETUP again.
In the user interface, under category Configuration files, you can set the filter Only changed keys (SITESETUP). Then only changed keys are displayed.
The dialog areas Comment for current installation and last changes are available in addition when SITESETUP is activated.
Comment for current installation
In the dialog area Comment for current installation, you can set comments for changes (reason of change for example)
Entries are
saved in the SITESETUP directory under $CADENAS_SITESETUP/configEditorUserIo.xml
.[25]
In the dialog area last changes the last value changes of the selected key are listed with their date.
With a click on an entry can be removed. When double-clicking on a value in the column Old values or New values this value is set again.
Entries are
saved in the SITESETUP directory under $CADENAS_SITESETUP/configEditorUserIo.xml
.[26]
Via "Conditions" you can easily specify
conditional sections in the start.env
for your installation
and so use different Setup directories. On this please see ???.
Under ? menu -> System info/Support (or F7 key) -> PARTsolutions variables you can also find §CADENAS_SITESETUP: The variable is linked to the corresponding directory. Simply click on it to get there. (You have to have the administrative rights for the respective directory.)