powered by CADENAS

Manual

Manual

4.5. Layout specifications

  • Top frame

    • Logo

      Your company logo is shown in the top frame on the left side.

      The logo should have the following specifications:

      File format: JPG, EPS, TIFF; maximum pixel size: 320 x 90

    • Buttons

      You can choose between two kinds of buttons:

      • CADENAS standard buttons

      • Company specific buttons

        Background color, border colorand icon color of the buttons can be specified as desired using hexadecimal or RGB values.

      Example

      Example

    • Background image

      Specify a background image or a background color as desired using hexadecimal or RGB values.

      File format: JPG; maximum pixel width: 1900 x 90

    • Font color

      The font/link color can be specified as desired using hexadecimal or RGB values.

    • Language icons

      The color, border color and background color of selected or not selected icons can be specified as desired using hexadecimal or RGB values.

      Selected and not selected icons

      Selected and not selected icons

  • Main frame

    • Design of tabulators

      Specify the active and passive tab color using hexadecimal or RGB values.

    • Design of tree structure

      Specify font color and background color of a selected line using hexadecimal or RGB values.

    • Design of tables

      Specify the background color of the selected line, mouseover line and clicked line using hexadecimal or RGB values.

  • E-Mail design

    This concerns info e-mails sent due to a lost password or activation e-mails, for example.

    • Color styles

      Specify the color of the headline, sub-headline and link using hexadecimal or RGB values.

      Specify the contact address.

    • Images

      Specify the company logo.

  • Start page

    [Hinweis] Hinweis

    ONLY for multiple catalogs or CAD/VAR portals!

    If you have ordered a multiple catalog or CAD/VAR portal, a specific start page will be set.

    • Specify the colors of the headline, line, text and link box using hexadecimal or RGB values.

      or

    • CANVAS will create all styles according to the style of your webpage.