Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.11.1. Registerseite
Allgemein
5.11.1.5. Show table row but hide LinkDB content -
plinkgroups.cfg -> [Role_name] -> Key "CONDITION"
|
|
---|---|
Zurück | Weiter |
Hinweis | |
---|---|
Filterbedingung für Datensätze is role dependent, so has to be defined for each role separately. |
Function: Show table row but hide LinkDB content. Reason could be data protection, if certain roles (users, departments) should not see certain information from the LinkDB. However, the row itself, they may see.
Setting in configuration file
$CADENAS_SETUP/plinkgroups.cfg
:
[Role_name]
CONDITION=(LINKTABLE.ACTIVE_STATE=1)
Meaning: Datasets which have the entry '1' in the ACTIVE_STATE column meet the condition. These table rows are displayed with all their LinkDB entries. Furthermore all other table rows without any LinkDB entries are displayed as well.
For LinkDB datasets wihich do not meet the condition the LinkDB content is hidden. However, the dataset itself is displayed.
Setting user interface under PARTadmin -> category Rollen -> Allgemein tab -> Filterbedingung für Datensätze
Zurück | Nach oben | Weiter |
5.11.1.4. Anzeigebedingung für Tabellenzeilen - plinkgroups.cfg -> Block [Role_name] -> Key "TABRESTRICTION" | Zum Anfang | 5.11.1.6. Anzuzeigende Spalten - plinkgroups.cfg -> Block [Role_name] -> Key "VARSUSED / VARSHIDDEN" |