![]() |
Valid syntax for attributes are:
Map a table variable into the given attribute
CadAttrName=?_ATTR("NB")
Map a VB expression into the given attribute, valid are also ?"3.1415926" ORELSE ?"This is a text"
CadAttrName=?AnyVBExpr
Attribute is mapped as value ORELSE as string
CadAttrName.Type=val|str
This is CAD-dependent information
CadAttrName.Custom=Any Custom Data
The Section "CopyFrom" also accepts complete statements .. the %ATTRNAME% is reduced by the current var
CopyFrom..=_FORMAT_0("MYPREFIX_HERE<ATTR-(%ATTRNAME%)>-MYPOST_HERE").value()
In addition, the "CopyFrom" may contain the following filter/flags:
Zurück | Nach oben | Weiter |
2.2.4.3. Werte-Typen | Zum Anfang | 2.2.4.5. Beispiele |