Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The configuration
file ifadeskinv.cfg
controls how the thread designation is translated from PARTsolutions to
Inventor.
As of V11 the
thread mapping is exclusively set via ifadeskinv.cfg
.
Threads are categorized in groups, which can be specified by regular expressions. Each group consists of key word and unique number.
ThreadGroupRx_10=M(\d+)(\.0*)?$ ThreadGroupRx_20=M(\d+ *\. *\d+)$ etc.
Another example: Thread mapping for M-threads which have a "x" in the name (e.g. M24x1)
ThreadGroupRx_30=M([0-9]+\.*[0-9]*) *x *([0-9]+\.*[0-9]*)
A search for a matching group is performed in ascending order. Subsequently it is checked whether the thread is available in one of the given tables separated by the specified decimal separator (see below). If a table with the searched thread is found, exactly this is used. Otherwise it is searched for another matching thread group. If a CADENAS thread matches a group, but can not be created with the data from this group in Inventor, then searching continues with the next group. If none of the given groups is matching, a respective error message is displayed.
Each group has to
have at least the keys ThreadGroupRx
and ThreadGroupTable
.
ThreadGroupRx
contains the
regular expression (see examples above).
ThreadGroupRx
is applied for
the CADENAS thread designation. If the expression matches the CADENAS
thread designation is transferred one-to-one to Inventor, where it is
searched in the thread.xls
.
ThreadGroupTable
is the
corresponding table's name in the thread.xls
.
All ThreadGroupTable
* keys do
support several table names separated by ";".
If there are tables with different decimal separators, then simply copy a group and adjust table name and separator (and other entries if needed).
ThreadGroupRx_70=ST(.+) ThreadGroupName_70=ST\1x%round(%pitch,1) ThreadGroupTable_70=THREADTBL_ISO_FORMING ThreadGroupClass_innerthread_70=6g ThreadGroupClass_outerhread_70=6g ThreadGroupDecimalMark_70=. ThreadGroupRx_71=ST(.+) ThreadGroupName_71=ST\1x%round(%pitch,1) ThreadGroupTable_71=THREADTBL_ISO_FORMING2 ThreadGroupClass_innerthread_71=6g ThreadGroupClass_outerhread_71=6g ThreadGroupDecimalMark_71=,
The decimal
separator for floating-point numbers is "." by default (if the key is
missing this is used). This setting can be overwritten with the global key
ThreadsDecimalMark
. In
addition, for each thread group the separator can be individually set via
constant ThreadGroupDecimalMark_xxx
(where
xxx is the thread group ID).
If the Inventor
designation name shall be different from the CADENAS designation name, then
the optional key ThreadGroupName
can be
set.
Available
variables for the creation of ThreadGroupName
:
Available
functions for the creation of ThreadGroupName
:
%ThreadDesignationMap_??? (??? stands for any but unique name): Changes thread diameters to values which can be handled by Inventor.
In the
ifadeskinv.cfg
exactly one matching line has to be available, which starts with
"ThreadDesignationMap_???=" and has value pairs separated by ";". These
value pairs then are used for the mapping. The values of a value pair
are separated by ",".
ThreadDesignationMap_UNx=0.06,0; 0.073,1; 0.086,2; 0.099,3; 0.112,4; 0.125,5; 0.138,6;0.164,8; 0.19,10; 0.216,12
%round: Returns a rounded value for the pitch. You can set the precision as second parameter optionally.
If the name for
inner and outer thread shall be different, then the keys ThreadGroupNameForInnerThread
and
ThreadGroupNameForOuterThread
have
to be used instead of ThreadGroupName
.
If there are
special tables for inner and outer thread, then instead of ThreadGroupTable
the keys
ThreadGroupTableForInnerThread
and
ThreadGroupTableForOuterThread
have to be used.
Furthermore the
self-explaining keys ThreadGroupTableForConic
and
ThreadGroupTableForNotConic
are
available as an alternative. Such a key can contain a direct reference to a
table in the thread.xls
or a reference to a table name in the ifadeskinv.cfg
.
If the threads are
sorted by classes in the table, then via ThreadGroupClass_innerthread
and
ThreadGroupClass_outerhread
the
respective class names for inner and outer thread can be set. If both keys
are not used then no class name is set. If only one class name shall be set,
regardless, you have to set both. Then the second key has to be
empty.
The pitch send to
Inventor can be set independently of the thread name (special case ST
threads). For this serves the key ThreadGroupPitch
. However, this
does not affect the variables %pitch and %invpitch.